We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Microchip’s High-Performance FPGA is First of its Kind to Achieve QML Class V in Ceramic Quad Flat Package

RTG4™ FPGAs offer a unique combination of radiation hardening by design, qualification to

QML Class V and packaging that simplifies board design, inspection and assembly


CHANDLER, Ariz., November 2, 2020 – Microchip Technology (Nasdaq: MCHP) today announced its RTG4™ Field Programmable Gate Array (FPGA) family is the first in a Ceramic Quad Flat Pack (CQFP) option to achieve qualification to the industry’s Qualified Manufacturers List (QML). The achievement will enable space system developers to create systems using more reliable packages that simplify the layout and routing of Printed Circuit Boards (PCBs) that are also easier to assemble and inspect.

“We have culminated years of testing, verification and flight heritage to offer a CQFP FPGA at the RTG4 FPGA density and performance level that is qualified to QML Class V, the highest reliability standard for spaceflight systems,” said Shakeel Peera, associate vice president of marketing for Microchip’s FPGA business unit. “Our high-speed radiation-tolerant RTG4 FPGAs were the first of their kind to achieve QML Class V qualification in any package type. They also were the first in their class to be offered in the 352-pin CQFP that is one of the most popular package types for space flight systems.”

Microchip’s CQFP package with 352 pins for RTG4 FPGAs simplifies system design in applications ranging from satellites and space probes to planet landers and vehicles. The CQFP package option is easier to assemble than Ceramic Column Grid Array packages, further improving reliability while enabling a more cost-effective system integration alternative to higher-pin-count alternatives. It is ideal for control applications that do not require a high number of inputs/outputs (I/Os) or need frequent switching and a high number of temperature cycles.

RTG4 FPGAs give space systems new high-speed signal-processing capabilities and leverage reprogrammable flash memory to provide greater immunity to configuration Single Event Upsets (SEUs) while consuming 40 to 50 percent less power than competing Static Random Access Memory (SRAM) FPGAs. RTG4 FPGAs feature 150,000 Logic Elements (LEs), 462 multipliers and 5.2 megabits (Mb) of memory. With this qualification, Microchip is now able to offer a full range of qualification and screening options for RTG4 FPGAs in the CQFP package suitable for a wide range of space missions from class 1 applications that require QML-V components, to low cost New Space constellations with relaxed screening requirements.

Please let us know if you would like to speak to a subject matter expert on Microchip’s RTG4 FPGAs and the significance of qualifying them to QML Class V in a CQFP for spaceflight applications.

PR image: https://www.flickr.com/photos/microchiptechnology/50514586712

Note: The Microchip name and logo and the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. RTG4 is a trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies. 

About Microchip Technology

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182
Reader Inquiries:

1-888-624-7435